Technical FAQs

Ask a Question

Does the CQO132M100CD Canadian load center have a Dual Rating?

Yes, the CQO132M100CD has a Dual Rating. It is CSA Approved, and UL Listed.


CTA-ID : 2039365
Was this helpful?
What can we do to improve the information ?