Technical FAQs

Ask a Question

Is the CQO124M100CD, Canadian load center, UL Listed?

Yes, the CQO124M100CD load center, has a Dual Rating. It is both UL Listed, and CSA Approved.


CTA-ID : 2039363
Was this helpful?
What can we do to improve the information ?