Technical FAQs

Ask a Question

Is there a vario switch and handle rated for installation into a nema 4/4X enclosure?

No, there is not a handle rated for a nema 4/4X environment. Our offering of the 9421V1W30 and 9421V2W30 enclosed nema 4/4X varios incorporate a modification that is not standard with an open switch. Since we don`t have a way to ensure that all the correct parts are used, we can`t make the statement.


CTA-ID : 2039727
Was this helpful?
What can we do to improve the information ?