Technical FAQs

Ask a Question

What are the shipping quantities on jumper part number AB1BE? What is 70 points sold in lots of 10?

The package quantity is 70 points per strip. These are sold only in lots of 10, for a total of 700 points.


CTA-ID : 2039098
Was this helpful?
What can we do to improve the information ?