Technical FAQs

Ask a Question

CH365R: Is this switch suitable for Service Entrance?

The CH365R is marked ``suitable for use as service equipment``.
The CH365R does not include a factory-installed neutral. If a neutral is required, order CH600SN. This neutral includes a neutral bonding screw. The neutral can be field-installed, and the neutral can be bonded in the field.

CTA-ID : 2039408
Was this helpful?
What can we do to improve the information ?