Technical FAQs

Ask a Question

What is the difference between a CQO140M200C and a CQO140M200CD, load center?

The CQO140M200C is only CSA approved and the CQO140M200CD is Dual rated, both CSA approved and UL Listed.


CTA-ID : 2039103
Was this helpful?
What can we do to improve the information ?