Technical FAQs

Ask a Question

Does the NQ panelboard have a 48 volt dc rating?

Issue:
DC rated panel

Product Line:
Panelboards

Environment:
NQ

Cause:
Rating

Resolution:
Yes, the QO/QOB branch breakers in the NQ panels  and any main  Powerpact H or J  or  Legacy LA breakers are rated at 48vdc , UL certified


CTA-ID : 2039810
Was this helpful?
What can we do to improve the information ?