Technical FAQs

Ask a Question

What is the meaning of suffix #1389 on Molded Case Switch catalog number KAL36000M1389?

The 1389 is an obsolete suffix that stands for a combination of 1212 1A/1B auxiliary switch, a 1200 alarm switch, and a 1021 240-120V shunt trip. Use 1395 suffix now. Original part number is replaced by a KHL36000M1395, which is on the system.

CTA-ID : 2040082
Was this helpful?
What can we do to improve the information ?