Technical FAQs

Ask a Question

What is the functional difference between the NQOD100SFL subfeed lug kit, and a QOB2125SL subfeed lug kit?

NQOD100SFL is a replacement figure 8 shaped lug which allows for two wires to loop into and out of the same lug. The QOB2125SL is a thermally and magnetically non protected breaker frame that plugs on the bus and allows for connection to the bus by means of lugs only. The QOB2125SL takes up breaker mounting space, while the NQOD100SFL does not.


CTA-ID : 2039778
Was this helpful?
What can we do to improve the information ?