Technical FAQs

Ask a Question

Is it permitted to land more than one wire under the terminals of a terminal block AB1VV235U?

No. The lugs on the AB1 terminal blocks are not rated for multiple conductors. One wire only is permitted.


CTA-ID : 2039147
Was this helpful?
What can we do to improve the information ?