Technical FAQs

Ask a Question

Is the RC2040M200CGP provided with a factory installed service disconnect?

Yes, a QOM2200VH utility main breaker is provided factory installed. A HOM230 back-fed generator breaker is also provided factory installed and is mechanically interlocked with the utility main breaker.

CTA-ID : 2039619
Was this helpful?
What can we do to improve the information ?