Technical FAQs

Ask a Question

What is the length of the shaft for the 9421LJ1?<br />

It is long enough to accomodate enclosures from 5 1/2 inches to 10 3/4 inches deep from the back of the door to the front of the back pan.


CTA-ID : 2039163
Was this helpful?
What can we do to improve the information ?