Technical FAQs

Ask a Question

Customer has panels being built with the UL 489 listed 240V M9 breakers and needs them to accept # 18 wire. The new catalog permits a minimum of #14.

A customer can pull #18 to UL 489 240 Vac breakers if they use a ring tongue terminal. The connector (customer supplied) must be UL Listed to accept #18 and it is a good idea to suggest that the connector is insulated. Also, the ring tongue can be used on the line and/or the load side.


CTA-ID : 2039142
Was this helpful?
What can we do to improve the information ?