Technical FAQs

Ask a Question

What is the temperature rating of the lugs on a HDL, HGL, HJL, HLL , HDA, HGA, HJA, HLA Circuit Breaker?

Product Line:
Circuit Breakers

Environment:
Electrical Distribution Equipment

Resolution:
The temperature rating is 75 degrees C.


CTA-ID : 2040796
Was this helpful?
What can we do to improve the information ?