Technical FAQs

Ask a Question

What hubs and knockouts are available to accommodate the Line Side Service conductors for a MP22125 meter stack?

Top endwall of a MP22125 unit will accommodate one Series A Hub
Catalog Numbers (Conduit Size): A100 (1``), A125 (1-1/4``), A150 (1-1/2``), A200 (2``), or A250 (2-1/2``).
Catalog Number: ACP (closing plate supplied factory installed).
Bottom endwall of a MP22125 uint is configured to accommodate one:
Catalog Number (Conduit Size): B300 (3``), or
Knockout ring sizes for Letter (Conduit Size):
A (1/2``) Service Ground
E (1-1/2``), F (2``), and G (2-1/2)


CTA-ID : 2039177
Was this helpful?
What can we do to improve the information ?