Technical FAQs

Ask a Question

Are the filters used on the shielded filter transformers such as 75T3HISFIL active or passive? <br /><br />REVISION R#2030440 (corrected typo in catalog number from 753THISFIL to 75T3HISFIL)

NOTE: The FIL fitler transformer product is NO LONGER AVAILABLE.
The filter units use a passive filter. They contain capacitive networks wired into the secondary and MOV arresters wired into primary.

CTA-ID : 2040887
Was this helpful?
What can we do to improve the information ?