Technical FAQs

Ask a Question

On the Uline starters what is the difference between the LUCA and the LUCB?

The difference between the Standard LUCA and the Advanced LUCB is the standard control unit provides only basic control and device state monitoring via the network communications, and the advanced units allow control, device state monitoring and data acquisition via network.

CTA-ID : 2039164
Was this helpful?
What can we do to improve the information ?