Technical FAQs

Ask a Question

Is it possible to convert an 82355R three pole double throw safety switch to a four pole double throw type in the field?

No. This type of conversion would void the UL listing of the device.


CTA-ID : 2040986
Was this helpful?
What can we do to improve the information ?