Technical FAQs

Ask a Question

Can a surge suppression unit catalog number TVS2EMA12A be mounted 40 feet away? What is the maximum distance of wire it can be connected with?

The maximum wire distance for the surge suppression units of this type is 3 feet, maximum. Greater distances of wire connection reduce the effectiveness of the surge suppression.

CTA-ID : 2040669
Was this helpful?
What can we do to improve the information ?