Technical FAQs

Ask a Question

Can you factory order a QO342MQB200 with a different amperage main circuit breaker?

Yes, you can Order with a differnt amperage main circuit breaker by changing the 200 to a different amperage, for example to order with a 100A main breaker, order a QO342MQB100. It is also listed with a 125A 150A and 175A main breaker.

CTA-ID : 2040803
Was this helpful?
What can we do to improve the information ?