Technical FAQs

Ask a Question

Do our duplex pump panels come with two circuit breaker disconnects?

Yes, two separate circuit breakers, or disconnect switches, with operators are included with all combination duplex motor controllers.


CTA-ID : 2040967
Was this helpful?
What can we do to improve the information ?