Technical FAQs

Ask a Question

What is the Terminal Lug Data for a 86325A Federal Pioneer General Duty safety switch?

The lugs on this device will accept (1) #1/0 AWG to 750 MCM copper or aluminum conductors per phase or (2) #1/0 AWG to 300 MCM copper or aluminum conductors per phase.


CTA-ID : 2040954
Was this helpful?
What can we do to improve the information ?