Technical FAQs

Ask a Question

What lug is available for the 400 amp LI breaker to accept parallel 3/0 conductors?

Use the CU600LI35 for two copper only wires ranging in size from #1awg to 350kcmil.


CTA-ID : 2040595
Was this helpful?
What can we do to improve the information ?