Technical FAQs

Ask a Question

SGA8180: Can the 5m (16.4 feet - suffix L05) and 10m (32.8 feet - suffix L10) cable be purchased separately?

No. The longer cables are factory installed only by adding the suffix L05 and L10 to the part number when ordering.

CTA-ID : 2040918
Was this helpful?
What can we do to improve the information ?