Technical FAQs

Ask a Question

What is the wire binding screw torque rating for a AL600LI35 lug?

Wire binding screw 300 lb-in. or 25 lb-ft.
Lug mounting screw 70 to 80 lb-in.


CTA-ID : 2040577
Was this helpful?
What can we do to improve the information ?