Technical FAQs

Ask a Question

What Equipment Ground Kit is used for the 400 and 600 AMP Heavy Duty Safety Switches (like a H366NR, Series E4)?

Issue:
Product Design features

Product Line:
Heavy Duty Safety Switches

Environment:
Ground kits

Cause:
Application

Resolution
ALL the 400 and 600amp Heavy Duty Safety Switches will use the PKOGTA2 ground kit.

NOTE: Two are required if equipment grounding conductors are run in parallel.


CTA-ID : 2040776
Was this helpful?
What can we do to improve the information ?