Technical FAQs

Ask a Question

Can a 9421LG1 opmech be used with a lower amperage GJL breaker; for example, a GJL36030 breaker?

Yes, there is a typo on page 8-13, Table 8.45 Digest 174. ``Frame size (A)`` 75,100. The correct labeling of the for the GJL Opmech should read 100 amps as the same frame is used for the lower amperage breakers.


CTA-ID : 2040917
Was this helpful?
What can we do to improve the information ?