Technical FAQs

Ask a Question

What is the part number for the legend included with the hand off auto kit 9999SC8?

While the actual legend provided with the kit is a 9001KN380, this is not generally available. A 9001KN360, a stock item, is the same as the KN380 except it is missing the international I and O markings. The 9001KN260 has similar marking to the KN360 but is smaller.


CTA-ID : 2040890
Was this helpful?
What can we do to improve the information ?