Technical FAQs

Ask a Question

What is the difference between limit switch bodies ZCKJ11 and ZCKJ1?

The ZCKJ1 has direct opening contacts but ZCKJ11 does not. The ZCKJ11 contact housing is a plug in unit, while the ZCKJ1 is not. The contact rating of the ZCKJ11 is NEMA A600 & Q600. The contact rating of the ZCKJ1 is NEMA A300 & Q300.

CTA-ID : 2040229
Was this helpful?
What can we do to improve the information ?