Technical FAQs

Ask a Question

2510FW2H: What is the replacement enclosure?

It is the 31056-080-51 (box) and 31057-529-50 (cover + gasket). If the device is a Series B, the box and cover can be replaced independently. If the device is Series A, both parts must be ordered. The new series is slightly wider and parts are not interchangeable.


CTA-ID : 2040392
Was this helpful?
What can we do to improve the information ?