Technical FAQs

Ask a Question

What size wires will fit into the neutral terminals in a 225 amp NQOD panel?<br />

The branch neutral terminals are suitable for #12-#4 aluminum and #14-#4 copper wires.


CTA-ID : 2040517
Was this helpful?
What can we do to improve the information ?