Technical FAQs

Ask a Question

What is the UL file number for power distribution connectors for FA, KA, LA, and MA type circuit breakers?

Issue:
What is the UL file number for  power distribution connectors for FA KA LA and MA circuit breakers?
PDC6FA6, PDC6KA4, PDC6LA20, PDC12LA4, PDC6MA20, PDC12MA4, PDC6HD6, PDC6JD4

Product Line:
Legacy circuit breakers

Environment:
Industrial control panels

Cause:
Customers require this information

Resolution:
These lugs are for use in UL 508 Industrial Control applications only, and are in UL file E10582, Volume W, Section 73.


CTA-ID : 2040365
Was this helpful?
What can we do to improve the information ?