Technical FAQs

Ask a Question

What are the part numbers for the lug covers for an MAL or MHL type circuit breaker?

48126-214-50 for the ``ON`` side of the breaker.
48126-497-50 for the ``OFF`` side.


CTA-ID : 2040303
Was this helpful?
What can we do to improve the information ?