Technical FAQs

Ask a Question

What is the difference between U and the E suffix version of the ATV11HU09M2?

The ``E`` suffix, which stands for European, only comes in 230V 1phase input only, it has the European current ratings not NEMA current ratings ie KW, and it has an intergrated EMC filter to meet the European CE requirements. The U suffix US version don`t have CE markings, available in 3phase or 1phase UL rated.


CTA-ID : 2038503
Was this helpful?
What can we do to improve the information ?