Technical FAQs

Ask a Question

What are the components of a VCF4?

V4 switch and KCF2PZ handle operator are the main components. There will also be a KZ74 interlock plate, KZ62 gasket, VZ18 shaft extension and a VZ9 terminal shield

CTA-ID : 2037406
Was this helpful?
What can we do to improve the information ?