Technical FAQs

Ask a Question

Are the Heavy Duty Receptacle Switches available in NEMA 7 & 9 enclosures?

No. This type of switch is available in NEMA 1, 3, 3R, 4, 4X, 5, 12 only.


CTA-ID : 2037972
Was this helpful?
What can we do to improve the information ?