Technical FAQs

Ask a Question

Can the existing thermistors from a Model 85 be used with the Model 98 retrofit kit?

The Model 98 retrofit kit comes with type K thermocouples which are different than thermistors . The Model 98 is designed to operate only with this type of thermocouple.


CTA-ID : 2038063
Was this helpful?
What can we do to improve the information ?