Technical FAQs

Ask a Question

What is the catalog number for the IP54 gasket and seals kit used with the XVEC21P?

XVEZ083 is IP54 gasket and seals for one beacon. XVEZ082 is the gasket and seals for five stack lights,the base, and the cover. XVEZ082 is included with the XVEC21P.

CTA-ID : 2038047
Was this helpful?
What can we do to improve the information ?