Technical FAQs

Ask a Question

How is the I-line TVSS unit wired when the source is a 480Y277 but they don`t pull a neutral to the I-line panelboard?

Connect the I-line TVSS unit neutral terminal to the TVSS ground terminal and bond the ground lug to the ground bus of the panel


CTA-ID : 2037997
Was this helpful?
What can we do to improve the information ?