Technical FAQs

Ask a Question

Can the handle padlock attachment that comes factory installed on a QOB3125VH circuit breaker be used to padlock the breaker in the on or off position?

The handle padlock attachment fits in a slot between the second and third poles of the three pole breaker. It can be used to padlock the device in either the ON or OFF position.

CTA-ID : 2037987
Was this helpful?
What can we do to improve the information ?