Technical FAQs

Ask a Question

On the 9001K56YM there is a tip that keeps the guard mounting flush. There is no hole in the enclosure to allow for the tip.

Issue:
On the 9001K56YM there is a tip that keeps the guard mounting flush.  There is no hole in the enclosure to allow for the tip.

Product Line:
30mm Push Button

Environment:
9001 K/SK 30mm push button

Cause:
To verify the installation instructions.                                                  

Resolution:                                                                 
This pin is an anti rotation pin. It is designed to keep the guard from rotating when the ring nut is tightened down on the guard. According to the instruction sheet you drill a hole in the enclosure for this pin. There is a gasket with the pin to seal the hole.
 
Was this helpful?
What can we do to improve the information ?