Technical FAQs

Ask a Question

Can you get a QO13842MX200, Intelligent load center, in 3-phase?

No, the Intelligent load centers, such as the QO13842MX200 is only available in single-phase.


CTA-ID : 2038345
Was this helpful?
What can we do to improve the information ?