Technical FAQs

Ask a Question

How do I order an L140 Cable Pull Switch? What are the options for the covers and mounting plates?

The options for the covers are: PF means transparent plastic cover, GF means transparent plastic with neon light and M means metal cover. The mounting plates are ``Style 1``, ``Style 2``, ``Style 3`` and ``Style 4``. Therefore, to order an L147 with a ``Style 2`` mounting plate and a metal cover the complete part number would be L1472M.

CTA-ID : 2037878
Was this helpful?
What can we do to improve the information ?