Technical FAQs

Ask a Question

What is the wire range for the neutral in catalog # Q23225NS?

The neutral accepts (1) #4-300kcmil. A PKOGTA2 ground kit is also included with this device. This kit consists of two lugs, suitable for #6 - 2/0 aluminum, or #10-2/0 copper conductors.

CTA-ID : 2037797
Was this helpful?
What can we do to improve the information ?