Technical FAQs

Ask a Question

What is the dB or decibel level and distance for the XVBC9M audible sounder?<br />

The XVBC9M audible sounder is adjustable from 75dB to 90 dB at a distance of 1 meter.





CTA-ID : 2037756
Was this helpful?
What can we do to improve the information ?