Technical FAQs

Ask a Question

Does the PAK10CTG come with a pedestal?

No, this device is not pedestal mounted. For a pedestal mounted device, consider using a PAK11PG, which includes an integral pedestal. The PAK11PG will have two receptacles fed by two QO120GFI breakers. The PAK10CTG is only supplied with one receptacle being fed by one QO120GFI.


CTA-ID : 2037721
Was this helpful?
What can we do to improve the information ?