Technical FAQs

Ask a Question

Is there a lock off feature for a GV2ME starter?

Yes. This feature is standard and is located in the Black starter button. By depressing the Red Stop button and pulling down the grey plastic piece under the Start button, a hole for the lock becomes visible.

CTA-ID : 2037587
Was this helpful?
What can we do to improve the information ?