Technical FAQs

Ask a Question

In catalog number QO612L100DTF, what is the significance of the ``D`` in the Catalogt number?

In this catalog number, ``D`` stands for a door on the cover. The Catalog number without the ``D`` would indicate an open front type load center, with no door on the cover. The branch circuit breaker handles would also be exposed.


CTA-ID : 2037484
Was this helpful?
What can we do to improve the information ?