Technical FAQs

Ask a Question

What is the available current range for the NC100H type supplementary protectors?

The NC100H breakers have an available current range from 10A to 80A. The currents are 10, 15, 16, 20, 25, 30, 32, 35, 40, 50, 60, 63, and 80A.


CTA-ID : 2037456
Was this helpful?
What can we do to improve the information ?