Technical FAQs

Ask a Question

What is the part number for a replacement plastic mounting nut for an 30mm Proximity switch?

The part number is a XSZE230. The kit contains [2] plastic jamnuts threaded for M30 x 1.5. Stainless steel jamnuts are available as P/N XSZE330.

CTA-ID : 2037377
Was this helpful?
What can we do to improve the information ?